Other Parts Discussed in Thread: LM5165,
Hello Team,
in the datasheet of the TPS54061 is written that Iq is 90uA (typ) under the following condition: Operating – Non switching.
What does it means Operating but not switching?
the datasheet describes:
The TPS54061 has a default startup voltage of approximately 4.5 V. The EN pin has an internal pullup current
source that can be used to adjust the input voltage UVLO threshold with two external resistors. In addition, the
pullup current provides a default condition. When the EN pin is floating the device will operate. The operating
current is 90 μA when not switching and under no load. When the device is disabled, the supply current is 1.4
μA.
what is the use case of being operating but not switching rather than being disabled?
The only thing that comes in my mind is that I have an high side switch following the DC-DC converter and it disables the circuitry following it.
I find that the way Iq is specified by the LM5165 is more comprehensive, simply from the description and not from the scenarios that it covers.
For consistency on the LM5165 I would have used "no load" and "with load" but also active let me think about loading the device.
- The TPS54061 Iq is the one that the LM5165 specifies as Iq sleep?
- What is the TPS54061 Iq typ. while the device output is loaded?
Having less specified parameters may let the TPS54061 being more cost efficient than the LM5165, but the description may be misleading.
thanks,
SunSet