Part Number: SM72295
Other Parts Discussed in Thread: INA213, INA240-Q1, INA240
Hello,
We have developed DC-DC Boost Converter in Current Controlled Mode, based on "SM72295 data sheet - Typical Application Circuit" with interface TI TMS320 microcontroller.
We need to sample this converter quickly to our customer so please provide the quick resolution for the same.
Based on the circuit (mentioned in data sheet) -
The PWM is running at 80KHz. Iout (max) = 6 Amps, Vout = 48Vdc, Vin = 20Vdc.
We are noticing that the current sense Amplifier Gain is not consistent for the range we tested as of now 0.25A to 3A, we expected gain to be 100 but the error is in 25-40% range.
(Vsense = 0.005E*6= 0.03 Vdc => Vout (Iout Pin) = 3 Vdc, which is connected to ADC of the uC).
Following are the experimental observation:
1. With Gain = 100 (R4=12K, R7=R8=120E), C8=100nF, C2=10nF, R15 = 0.005E
(a) for PWM=80KHz - Error was in 25-40% for 0.25A to 2A range.
(b) With Bypass Mode (i.e. PWM not working) there is only 1% error at Iout pin for 0.25A to 2A range.
2. With Gain = 17.5 (R4=8.25K, R7=R8=470E), C8=100nF, C2=10nF, R15 = 0.005E
(a) for PWM = 80KHz => Errors are in 25% range started from load current >1.5A
(b) for PWM = 40KHz => Errors are in 14% range from load current >2.75A
Please find attached XLS for the readings.
Thanks in advance for providing quick resolutions!
--AshishSM27795_Current_Sense.xlsx