Other Parts Discussed in Thread: UC2709
Hi All,
So I am developing a new design for an application and previously had great success with the UC2709 driver. Now, trying to do my due dilligence for obsolence I quickly realized this part was designed a long time ago and it would behoove me to try out new drivers. This led me to to try out the UCC27524 non inverting gate driver. I don't have a shcematic for you but let me be as despcriptive as I can be.
I am powering the DIP version of this part on a small breadboard with 15V from a benchtop power supply connected to pin 6 and ground connected to pin 3. I am using an Artix-7 CMOD35T development board to drive one(eventually two, 90 out of phase) I/O with 3.3V TTL pulses at 2MHz. I have a common ground connection between the device, FPGA, and power supply.
Some obervations:
- First, with no inputs the device draws 1mA.
- When I run the FPGA routine, and have one output connected to pin 2(INA) the device does not draw any more current. I verified with an oscilloscope that the signal from the FPGA is okay. The output from OUTA is nothing at all.
- The same result is obtained when I use a benchtop function generator with 3.3V or 5.5V TTL pulses as well.
I ordered a batch of 10 of these from Digikey and have frustratingly had no success. With the UC2709 I had no issues with this setup. I also realize that perhaps I may benefit from using decoupling capacitors but this does not seem to explain the behavior I'm seeing.
Is it possible I have a bad batch of devices or I am making a mistake with my test setup? Let me know if i can provide details that will help me to resolve my issue. Thank you!