Hi
My customer is currently reviewing the Power switch for Cradle.
I am looking for the following power switch:
1. Input voltage: 5V
2. Rated current: 1.5A ~ 2A
3. Adjustable current limit
- When the set limit value is exceeded, output voltage output is maintained,
Current is used up to the set value.
4. Over voltage protection
When I looked at it, it was TPS25925x. I want to know if the product is suitable.
Looking at Figure 38 in the datasheet below, it is understood that Vout will drop only as much as the body diode if current increases by 125%. Is that what I understood?
Or can you recommend a better product?