This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24190: BQ24190 Not Charging

Part Number: BQ24190

Hi I have a BQ24190 connected to a Lithium Ion Battery.

Battery Voltage is 3.6V

After connecting adaptor, It is not charging the battery.

The register values are are below in hex from 00 to 0A

35 1B 60 11 B2 9A 03 4B 84 00 23