I'm trying to generate less than .8 volts with the LMZ23605 Simple Switcher. I have a negative voltage rail. My questions are:
1. Can this be done?
2. If not, Why?
3. If this was attempted, what would be the behavior of the device? In other words, what would the output regulate to?
From the block diagram in the data sheet, it seems this should be possible considering the FB node is closing the internal erroramp FB loop.
Surly the device will be in dcm mode at this extemely low voltage, but an average value should be attainable with excessive filtering (bigs-ass Vo cap).