Part Number: TPS63024
Hi team,
The customer measured the minimum voltage of L2 pin at the boost operation is -0.8V,
The L2 absolute voltage in datasheet is -0.3V and note says (4) AC transient voltage rating, so -0.8V is over the absolute voltage
My understanding is that the inductor tries to sustain the current when the internal N - FET goes from ON to OFF, so the L2 voltage will be -0.8 V due to the body diode or ESD.
I would like to confirm what mean the -0.3V of Absolute Maximum Ratings?
Regards,
Ogasawara