This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63024: L2 pin minimum absolute voltage

Part Number: TPS63024

Hi team,

 The customer measured the minimum voltage of L2 pin at the boost operation is -0.8V,

 The L2 absolute voltage in datasheet is -0.3V and note says (4) AC transient voltage rating, so -0.8V is over the absolute voltage
 My understanding is that the inductor tries to sustain the current when the internal N - FET goes from ON to OFF, so the L2 voltage will be -0.8 V due to the body diode or ESD.

 I would like to confirm what mean the -0.3V of Absolute Maximum Ratings?

Regards,

Ogasawara