The datasheet says that the AD for internal and external temperature measurement is 16 bits, and the measurement range is 0-6553.5 ºK.
For the actual simulation test, the external temperature measurement was used, the open circuit temperature resistance was -39 °C, and the short circuit temperature resistance was shown to be 123 °C.
Can we adjust the temperature display range to at least -55~125°C or higher? (The temperature probe is actually used as 103F3435, which is very close to the AT103 parameter recommended in the specification. The parameter list is given as -55~125°C)