This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61158: Measure LED current produced by TPS61158 with INA139

Part Number: TPS61158
Other Parts Discussed in Thread: INA139

Is it possible to attach a INA139 (Hi-Side Current Shunt Monitor) parallel to the feedback resistor of the TPS61158 WLED driver as shown below?

I'd like to use PWM for Dimming and need to measure the resulting current.But I do not know, if the INA139 sees a constant voltage or a rectangle or sawtooth waveform, when applying PWM with approx. 100kHz. I assume, that the additional resistive load from the INA139 does not disturb the regulation of the TPS61158.