Part Number: CSD19505KTT
Other Parts Discussed in Thread: TIDA-00792, CSD19536KTT
Hello everybody,
I wanted to build a battery management system. Because I am not very expierenced in building these systems I used the TIDA-00792 (sheet 1) reference design and changed the CSD19536KTT into CSD19505KTT. The other three sheets of TIDA-00792 I did not respected. After finishing the schematic I designed the pcb of my own.
While testing the discharge direction I have the problem that one of the two DSG mosfet is not working properly while leading 10A over all current. In the low currents tests I did not have any problems leading. After having this issue, I measured the transit resistance. I observed that one of these mosfet had an low-ohmic source-drain resistance. Therefore I replaced the damaged mosfet and started the measurement again, but now with a thermal camera. I noticed that one of the source-connecting tracks had a lot more thermal burden than the other. I took a look at the layout and saw that the track width is noticeable different. Can this difference cause the problem? While reasearch I often read about oscillation problems coused through incorrect routing. But I also placed the 200R ferrite bead infront of every mosfet corresponding to the reference design.
Finally I made an measurement using only one MOSFET each side, and I had no errors (only high track warming).
It would by glad, if you would share your ideas with me!
Thanks,
Max