Other Parts Discussed in Thread: LM5069, TPS25942A, TPS2660
Hello,
Am using LM5060. As per the calculation sheet available from texas, the minimum worst case over current threshold : 3.5A,
Max worst case over current threshold : 26.3A.
The threshold (Min to Max) are not linear. Kindly provide information regarding this.
Also suggest whether the threshold can be tunable to the nearest values (Min 3.5A & Max 26.3A is very high).