Other Parts Discussed in Thread: TPS62160, TPS62821, TPS62802
I would like to know if the TPS62125 can handle pulse current over it's steady operating limit.
The worse case scenario is 25ms at 500mA at 3.3v. This event will occur at most every 8 seconds, but typically does not happen.
The device is normally operating the <300mA limit. The device’s input is 5V - 3.3 V.
The device presently operates fine, but would it fail in the future or this 25ms short pulse of 500mA is acceptable .
Thanks