Other Parts Discussed in Thread: GPCCHEM, BQSTUDIO, EV2400
Hi,
I developped a program in order to initialise the bq27441.
I have modified the specifics settings like asked in the datasheet :
> Design Capacity (DC) : 3300
> Design Energy(Dnrj) : 12210
> Terminate Voltage(TVolt) : 3200
> Taper Rate(TR) : 330
However, my RM never reach the maximal value (3300) when the battery is full. It maximal values match with 60% of the DC. Also, when SOC reach 0% my battery is not empty.
For exemple, when my battery is full, I have 1724 as RM value and 3107 for Full Available Capacity value.
When I decrease the value of DC, the RM value decrease too and it's not logical.. I think that the RM value must be the same!
Hypothesis:
> When my battery charging, it is disconected from the bq27441, it's a problem?
> My battery is an Lithium-Polymer Battery, Need I to modified something for this?
Thanks,
Cédric