This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50: BQ40Z50 i2c issue

Part Number: BQ40Z50

Hi Team,

My customer is using BQ40Z50, but they now can't communicate with BQ40Z50 through I2C. Below is the debug summary for your check, would you pls help look into this issue?

BQ40Z50 debug software configuration.docx

The reference code is from TI website, the code as below:

/*
 * bq40z50 fuel gauge driver
 *
 * Copyright (C) 2017 Texas Instruments Incorporated - http://www.ti.com/
 *
 * This program is free software; you can redistribute it and/or
 * modify it under the terms of the GNU General Public License version 2 as
 * published by the Free Software Foundation.
 *
 * This program is distributed "as is" WITHOUT ANY WARRANTY of any
 * kind, whether express or implied; without even the implied warranty
 * of MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
 * GNU General Public License for more details.
 */

#define pr_fmt(fmt)	"[bq40z50] %s: " fmt, __func__
#include <linux/module.h>
#include <linux/param.h>
#include <linux/jiffies.h>
#include <linux/workqueue.h>
#include <linux/delay.h>
#include <linux/platform_device.h>
#include <linux/power_supply.h>
#include <linux/i2c.h>
#include <linux/slab.h>
#include <linux/uaccess.h>
#include <linux/interrupt.h>
#include <linux/gpio/consumer.h>

#define bq_info	pr_info
#define bq_dbg	pr_debug
#define bq_err	pr_err
#define bq_log	pr_err


#define	INVALID_REG_ADDR	0xFF

#define FG_FLAGS_FD				BIT(4)
#define	FG_FLAGS_FC				BIT(5)
#define	FG_FLAGS_DSG				BIT(6)
#define FG_FLAGS_RCA				BIT(9)


enum bq_fg_reg_idx {
	BQ_FG_REG_MAC = 0,
	BQ_FG_REG_TEMP,		/* Battery Temperature */
	BQ_FG_REG_VOLT,		/* Battery Voltage */
	BQ_FG_REG_AI,		/* Average Current */
	BQ_FG_REG_BATT_STATUS,	/* BatteryStatus */
	BQ_FG_REG_TTE,		/* Time to Empty */
	BQ_FG_REG_TTF,		/* Time to Full */
	BQ_FG_REG_FCC,		/* Full Charge Capacity */
	BQ_FG_REG_RM,		/* Remaining Capacity */
	BQ_FG_REG_CC,		/* Cycle Count */
	BQ_FG_REG_SOC,		/* Relative State of Charge */
	BQ_FG_REG_SOH,		/* State of Health */
	BQ_FG_REG_DC,		/* Design Capacity */
	BQ_FG_REG_MBA,		/* ManufacturerBlockAccess*/
	NUM_REGS,
};

enum bq_fg_mac_cmd {
	FG_MAC_CMD_OP_STATUS	= 0x0000,
	FG_MAC_CMD_DEV_TYPE	= 0x0001,
	FG_MAC_CMD_FW_VER	= 0x0002,
	FG_MAC_CMD_HW_VER	= 0x0003,
	FG_MAC_CMD_IF_SIG	= 0x0004,
	FG_MAC_CMD_CHEM_ID	= 0x0006,
	FG_MAC_CMD_GAUGING	= 0x0021,
	FG_MAC_CMD_SEAL		= 0x0030,
	FG_MAC_CMD_DEV_RESET	= 0x0041,
};


enum {
	SEAL_STATE_RSVED,
	SEAL_STATE_UNSEALED,
	SEAL_STATE_SEALED,
	SEAL_STATE_FA,
};


enum bq_fg_device {
	BQ40Z50,
};

static const unsigned char *device2str[] = {
	"bq40z50",
};

static u8 bq40z50_regs[NUM_REGS] = {
	0x00,	/* CONTROL */
	0x08,	/* TEMP */
	0x09,	/* VOLT */
	0x0B,	/* AVG CURRENT */
	0x16,	/* FLAGS */
	0x12,	/* Time to empty */
	0x13,	/* Time to full */
	0x10,	/* Full charge capacity */
	0x0F,	/* Remaining Capacity */
	0x17,	/* CycleCount */
	0x0D,	/* State of Charge */
	0x4F,	/* State of Health */
	0x18,	/* Design Capacity */
	0x44,	/* ManufacturerBlockAccess*/
};

struct bq_fg_chip {
	struct device *dev;
	struct i2c_client *client;


	struct mutex i2c_rw_lock;
	struct mutex data_lock;
	struct mutex irq_complete;

	bool irq_waiting;
	bool irq_disabled;
	bool resume_completed;

	int fw_ver;
	int df_ver;

	u8 chip;
	u8 regs[NUM_REGS];

	/* status tracking */

	bool batt_fc;
	bool batt_fd;	/* full depleted */

	bool batt_dsg;
	bool batt_rca;	/* remaining capacity alarm */

	int seal_state; /* 0 - Full Access, 1 - Unsealed, 2 - Sealed */
	int batt_tte;
	int batt_soc;
	int batt_fcc;	/* Full charge capacity */
	int batt_rm;	/* Remaining capacity */
	int batt_dc;	/* Design Capacity */
	int batt_volt;
	int batt_temp;
	int batt_curr;

	int batt_cyclecnt;	/* cycle count */

	/* debug */
	int skip_reads;
	int skip_writes;

	int fake_soc;
	int fake_temp;

	struct	delayed_work monitor_work;

	struct power_supply *fg_psy;
	struct power_supply_desc fg_psy_d;
};


static int __fg_read_word(struct i2c_client *client, u8 reg, u16 *val)
{
	s32 ret;

	ret = i2c_smbus_read_word_data(client, reg);
	if (ret < 0) {
		bq_err("i2c read word fail: can't read from reg 0x%02X\n", reg);
		return ret;
	}

	*val = (u16)ret;

	return 0;
}


static int __fg_write_word(struct i2c_client *client, u8 reg, u16 val)
{
	s32 ret;

	ret = i2c_smbus_write_word_data(client, reg, val);
	if (ret < 0) {
		bq_err("i2c write word fail: can't write 0x%02X to reg 0x%02X\n",
				val, reg);
		return ret;
	}

	return 0;
}

static int __fg_read_block(struct i2c_client *client, u8 reg, u8 *buf, u8 len)
{

	int ret;

	/* len is ignored due to smbus block reading contains Num of bytes to be returned */
	ret = i2c_smbus_read_block_data(client, reg, buf);

	return ret;
}

static int __fg_write_block(struct i2c_client *client, u8 reg, u8 *buf, u8 len)
{
	int ret;

	ret = i2c_smbus_write_block_data(client, reg, len, buf);

	return ret;
}

static int fg_read_word(struct bq_fg_chip *bq, u8 reg, u16 *val)
{
	int ret;

	if (bq->skip_reads) {
		*val = 0;
		return 0;
	}

	mutex_lock(&bq->i2c_rw_lock);
	ret = __fg_read_word(bq->client, reg, val);
	mutex_unlock(&bq->i2c_rw_lock);

	return ret;
}

static int fg_write_word(struct bq_fg_chip *bq, u8 reg, u16 val)
{
	int ret;

	if (bq->skip_writes)
		return 0;

	mutex_lock(&bq->i2c_rw_lock);
	ret = __fg_write_word(bq->client, reg, val);
	mutex_unlock(&bq->i2c_rw_lock);

	return ret;
}

static int fg_read_block(struct bq_fg_chip *bq, u8 reg, u8 *buf, u8 len)
{
	int ret;

	if (bq->skip_reads)
		return 0;
	mutex_lock(&bq->i2c_rw_lock);
	ret = __fg_read_block(bq->client, reg, buf, len);
	mutex_unlock(&bq->i2c_rw_lock);

	return ret;

}

static int fg_write_block(struct bq_fg_chip *bq, u8 reg, u8 *data, u8 len)
{
	int ret;

	if (bq->skip_writes)
		return 0;

	mutex_lock(&bq->i2c_rw_lock);
	ret = __fg_write_block(bq->client, reg, data, len);
	mutex_unlock(&bq->i2c_rw_lock);

	return ret;
}

static u8 checksum(u8 *data, u8 len)
{
	u8 i;
	u16 sum = 0;

	for (i = 0; i < len; i++)
		sum += data[i];

	sum &= 0xFF;

	return 0xFF - sum;
}

#if 0
static void fg_print_buf(const char *msg, u8 *buf, u8 len)
{
	int i;
	int idx = 0;
	int num;
	u8 strbuf[128];

	bq_err("%s buf: ", msg);
	for (i = 0; i < len; i++) {
		num = sprintf(&strbuf[idx], "%02X ", buf[i]);
		idx += num;
	}
	bq_err("%s\n", strbuf);
}
#else
static void fg_print_buf(const char *msg, u8 *buf, u8 len)
{}
#endif

static int fg_mac_read_block(struct bq_fg_chip *bq, u16 cmd, u8 *buf, u8 len)
{
	int ret;
	u8 t_buf[40];
	u8 t_len;
	int i;

	t_buf[0] = (u8)(cmd >> 8);
	t_buf[1] = (u8)cmd;
	ret = fg_write_block(bq, bq->regs[BQ_FG_REG_MBA], t_buf, 2);
	if (ret < 0)
		return ret;

	msleep(100);

	ret = fg_read_block(bq, bq->regs[BQ_FG_REG_MBA], t_buf, 36);
	if (ret < 0)
		return ret;
	t_len = ret;
	/* ret contains number of data bytes in gauge's response*/
	fg_print_buf("mac_read_block", t_buf, t_len);

	for (i = 0; i < t_len - 2; i++)
		buf[i] = t_buf[i+2];

	return 0;
}

#if 0
static int fg_mac_write_block(struct bq_fg_chip *bq, u16 cmd, u8 *data, u8 len)
{
	int ret;
	u8 cksum;
	u8 t_buf[40];
	int i;

	if (len > 32)
		return -1;

	t_buf[0] = (u8)(cmd >> 8);
	t_buf[1] = (u8)cmd;
	for (i = 0; i < len; i++)
		t_buf[i+2] = data[i];

	/*write command/addr, data*/
	ret = fg_write_block(bq, bq->regs[BQ_FG_REG_MBA], t_buf, len + 2);
	if (ret < 0)
		return ret;

	return ret;
}
#endif

static void fg_read_fw_version(struct bq_fg_chip *bq)
{

	int ret;
	u8 buf[36];

	ret = fg_write_word(bq, bq->regs[BQ_FG_REG_MBA], FG_MAC_CMD_FW_VER);

	if (ret < 0) {
		bq_err("Failed to send firmware version subcommand:%d\n", ret);
		return;
	}

	mdelay(2);

	ret = fg_mac_read_block(bq, bq->regs[BQ_FG_REG_MBA], buf, 11);
	if (ret < 0) {
		bq_err("Failed to read firmware version:%d\n", ret);
		return;
	}

	bq_log("FW Ver:%04X, Build:%04X\n",
		buf[2] << 8 | buf[3], buf[4] << 8 | buf[5]);
	bq_log("Ztrack Ver:%04X\n", buf[7] << 8 | buf[8]);
}


static int fg_read_status(struct bq_fg_chip *bq)
{
	int ret;
	u16 flags;

	ret = fg_read_word(bq, bq->regs[BQ_FG_REG_BATT_STATUS], &flags);
	if (ret < 0)
		return ret;

	mutex_lock(&bq->data_lock);
	bq->batt_fc		= !!(flags & FG_FLAGS_FC);
	bq->batt_fd		= !!(flags & FG_FLAGS_FD);
	bq->batt_rca		= !!(flags & FG_FLAGS_RCA);
	bq->batt_dsg		= !!(flags & FG_FLAGS_DSG);
	mutex_unlock(&bq->data_lock);

	return 0;
}


static int fg_read_rsoc(struct bq_fg_chip *bq)
{
	int ret;
	u16 soc = 0;

	ret = fg_read_word(bq, bq->regs[BQ_FG_REG_SOC], &soc);
	if (ret < 0) {
		bq_err("could not read RSOC, ret = %d\n", ret);
		return ret;
	}

	return soc;

}

static int fg_read_temperature(struct bq_fg_chip *bq)
{
	int ret;
	u16 temp = 0;

	ret = fg_read_word(bq, bq->regs[BQ_FG_REG_TEMP], &temp);
	if (ret < 0) {
		bq_err("could not read temperature, ret = %d\n", ret);
		return ret;
	}

	return temp - 2730;

}

static int fg_read_volt(struct bq_fg_chip *bq)
{
	int ret;
	u16 volt = 0;

	ret = fg_read_word(bq, bq->regs[BQ_FG_REG_VOLT], &volt);
	if (ret < 0) {
		bq_err("could not read voltage, ret = %d\n", ret);
		return ret;
	}

	return volt;

}

static int fg_read_current(struct bq_fg_chip *bq, int *curr)
{
	int ret;
	u16 avg_curr = 0;

	ret = fg_read_word(bq, bq->regs[BQ_FG_REG_AI], &avg_curr);
	if (ret < 0) {
		bq_err("could not read current, ret = %d\n", ret);
		return ret;
	}
	*curr = (int)((s16)avg_curr);

	return ret;
}

static int fg_read_fcc(struct bq_fg_chip *bq)
{
	int ret;
	u16 fcc;

	if (bq->regs[BQ_FG_REG_FCC] == INVALID_REG_ADDR) {
		bq_err("FCC command not supported!\n");
		return 0;
	}

	ret = fg_read_word(bq, bq->regs[BQ_FG_REG_FCC], &fcc);

	if (ret < 0)
		bq_err("could not read FCC, ret=%d\n", ret);

	return fcc;
}

static int fg_read_dc(struct bq_fg_chip *bq)
{

	int ret;
	u16 dc;

	if (bq->regs[BQ_FG_REG_DC] == INVALID_REG_ADDR) {
		bq_err("DesignCapacity command not supported!\n");
		return 0;
	}

	ret = fg_read_word(bq, bq->regs[BQ_FG_REG_DC], &dc);

	if (ret < 0) {
		bq_err("could not read DC, ret=%d\n", ret);
		return ret;
	}

	return dc;
}


static int fg_read_rm(struct bq_fg_chip *bq)
{
	int ret;
	u16 rm;

	if (bq->regs[BQ_FG_REG_RM] == INVALID_REG_ADDR) {
		bq_err("RemainingCapacity command not supported!\n");
		return 0;
	}

	ret = fg_read_word(bq, bq->regs[BQ_FG_REG_RM], &rm);

	if (ret < 0) {
		bq_err("could not read DC, ret=%d\n", ret);
		return ret;
	}

	return rm;

}

static int fg_read_cyclecount(struct bq_fg_chip *bq)
{
	int ret;
	u16 cc;

	if (bq->regs[BQ_FG_REG_CC] == INVALID_REG_ADDR) {
		bq_err("Cycle Count not supported!\n");
		return -1;
	}

	ret = fg_read_word(bq, bq->regs[BQ_FG_REG_CC], &cc);

	if (ret < 0) {
		bq_err("could not read Cycle Count, ret=%d\n", ret);
		return ret;
	}

	return cc;
}

static int fg_read_tte(struct bq_fg_chip *bq)
{
	int ret;
	u16 tte;

	if (bq->regs[BQ_FG_REG_TTE] == INVALID_REG_ADDR) {
		bq_err("Time To Empty not supported!\n");
		return -1;
	}

	ret = fg_read_word(bq, bq->regs[BQ_FG_REG_TTE], &tte);

	if (ret < 0) {
		bq_err("could not read Time To Empty, ret=%d\n", ret);
		return ret;
	}

	if (ret == 0xFFFF)
		return -ENODATA;

	return tte;
}

static int fg_get_batt_status(struct bq_fg_chip *bq)
{

	fg_read_status(bq);

	if (bq->batt_fc)
		return POWER_SUPPLY_STATUS_FULL;
	else if (bq->batt_dsg)
		return POWER_SUPPLY_STATUS_DISCHARGING;
	else if (bq->batt_curr > 0)
		return POWER_SUPPLY_STATUS_CHARGING;
	else
		return POWER_SUPPLY_STATUS_NOT_CHARGING;

}


static int fg_get_batt_capacity_level(struct bq_fg_chip *bq)
{

	if (bq->batt_fc)
		return POWER_SUPPLY_CAPACITY_LEVEL_FULL;
	else if (bq->batt_rca)
		return POWER_SUPPLY_CAPACITY_LEVEL_LOW;
	else if (bq->batt_fd)
		return POWER_SUPPLY_CAPACITY_LEVEL_CRITICAL;
	else
		return POWER_SUPPLY_CAPACITY_LEVEL_NORMAL;

}


static enum power_supply_property fg_props[] = {
	POWER_SUPPLY_PROP_STATUS,
	POWER_SUPPLY_PROP_PRESENT,
	POWER_SUPPLY_PROP_VOLTAGE_NOW,
	POWER_SUPPLY_PROP_CURRENT_NOW,
	POWER_SUPPLY_PROP_CAPACITY,
	POWER_SUPPLY_PROP_CAPACITY_LEVEL,
	POWER_SUPPLY_PROP_TEMP,
	/*POWER_SUPPLY_PROP_HEALTH,*//*implement it in battery power_supply*/
	POWER_SUPPLY_PROP_CHARGE_FULL,
	POWER_SUPPLY_PROP_TECHNOLOGY,
	POWER_SUPPLY_PROP_RESISTANCE_ID,
	POWER_SUPPLY_PROP_UPDATE_NOW,
};

static int fg_get_property(struct power_supply *psy, enum power_supply_property psp,
					union power_supply_propval *val)
{
	struct bq_fg_chip *bq = power_supply_get_drvdata(psy);
	int ret;

	switch (psp) {
	case POWER_SUPPLY_PROP_STATUS:
		val->intval = fg_get_batt_status(bq);
		break;
	case POWER_SUPPLY_PROP_VOLTAGE_NOW:
		ret = fg_read_volt(bq);
		mutex_lock(&bq->data_lock);
		if (ret >= 0)
			bq->batt_volt = ret;
		val->intval = bq->batt_volt * 1000;
		mutex_unlock(&bq->data_lock);

		break;
	case POWER_SUPPLY_PROP_PRESENT:
		val->intval = 1;
		break;
	case POWER_SUPPLY_PROP_CURRENT_NOW:
		mutex_lock(&bq->data_lock);
		fg_read_current(bq, &bq->batt_curr);
		val->intval = -bq->batt_curr * 1000;
		mutex_unlock(&bq->data_lock);
		break;

	case POWER_SUPPLY_PROP_CAPACITY:
		if (bq->fake_soc >= 0) {
			val->intval = bq->fake_soc;
			break;
		}
		ret = fg_read_rsoc(bq);
		mutex_lock(&bq->data_lock);
		if (ret >= 0)
			bq->batt_soc = ret;
		val->intval = bq->batt_soc;
		mutex_unlock(&bq->data_lock);
		break;

	case POWER_SUPPLY_PROP_CAPACITY_LEVEL:
		val->intval = fg_get_batt_capacity_level(bq);
		break;

	case POWER_SUPPLY_PROP_TEMP:
		if (bq->fake_temp != -EINVAL) {
			val->intval = bq->fake_temp;
			break;
		}
		ret = fg_read_temperature(bq);
		mutex_lock(&bq->data_lock);
		if (ret > 0)
			bq->batt_temp = ret;
		val->intval = bq->batt_temp;
		mutex_unlock(&bq->data_lock);
		break;

	case POWER_SUPPLY_PROP_TIME_TO_EMPTY_NOW:
		ret = fg_read_tte(bq);
		mutex_lock(&bq->data_lock);
		if (ret >= 0)
			bq->batt_tte = ret;

		val->intval = bq->batt_tte;
		mutex_unlock(&bq->data_lock);
		break;

	case POWER_SUPPLY_PROP_CHARGE_FULL:
		ret = fg_read_fcc(bq);
		mutex_lock(&bq->data_lock);
		if (ret > 0)
			bq->batt_fcc = ret;
		val->intval = bq->batt_fcc * 1000;
		mutex_unlock(&bq->data_lock);
		break;

	case POWER_SUPPLY_PROP_CHARGE_FULL_DESIGN:
		ret = fg_read_dc(bq);
		mutex_lock(&bq->data_lock);
		if (ret > 0)
			bq->batt_dc = ret;
		val->intval = bq->batt_dc * 1000;
		mutex_unlock(&bq->data_lock);
		break;

	case POWER_SUPPLY_PROP_CYCLE_COUNT:
		ret = fg_read_cyclecount(bq);
		mutex_lock(&bq->data_lock);
		if (ret >= 0)
			bq->batt_cyclecnt = ret;
		val->intval = bq->batt_cyclecnt;
		mutex_unlock(&bq->data_lock);
		break;

	case POWER_SUPPLY_PROP_TECHNOLOGY:
		val->intval = POWER_SUPPLY_TECHNOLOGY_LIPO;
		break;

	case POWER_SUPPLY_PROP_RESISTANCE_ID:
		val->intval = 0;
		break;
	case POWER_SUPPLY_PROP_UPDATE_NOW:
		val->intval = 0;
		break;

	default:
		return -EINVAL;
	}
	return 0;
}
static void fg_dump_registers(struct bq_fg_chip *bq);

static int fg_set_property(struct power_supply *psy,
			       enum power_supply_property prop,
			       const union power_supply_propval *val)
{
	struct bq_fg_chip *bq = power_supply_get_drvdata(psy);

	switch (prop) {
	case POWER_SUPPLY_PROP_TEMP:
		bq->fake_temp = val->intval;
		break;
	case POWER_SUPPLY_PROP_CAPACITY:
		bq->fake_soc = val->intval;
		power_supply_changed(bq->fg_psy);
		break;
	case POWER_SUPPLY_PROP_UPDATE_NOW:
		fg_dump_registers(bq);
		break;
	default:
		return -EINVAL;
	}

	return 0;
}


static int fg_prop_is_writeable(struct power_supply *psy,
				       enum power_supply_property prop)
{
	int ret;

	switch (prop) {
	case POWER_SUPPLY_PROP_TEMP:
	case POWER_SUPPLY_PROP_CAPACITY:
	case POWER_SUPPLY_PROP_UPDATE_NOW:
		ret = 1;
		break;
	default:
		ret = 0;
		break;
	}
	return ret;
}



static int fg_psy_register(struct bq_fg_chip *bq)
{
	struct power_supply_config fg_psy_cfg = {};

	bq->fg_psy_d.name = "bms";
	bq->fg_psy_d.type = POWER_SUPPLY_TYPE_BMS;
	bq->fg_psy_d.properties = fg_props;
	bq->fg_psy_d.num_properties = ARRAY_SIZE(fg_props);
	bq->fg_psy_d.get_property = fg_get_property;
	bq->fg_psy_d.set_property = fg_set_property;
	bq->fg_psy_d.property_is_writeable = fg_prop_is_writeable;

	fg_psy_cfg.drv_data = bq;
	fg_psy_cfg.num_supplicants = 0;
	bq->fg_psy = devm_power_supply_register(bq->dev,
						&bq->fg_psy_d,
						&fg_psy_cfg);
	if (IS_ERR(bq->fg_psy)) {
		bq_err("Failed to register fg_psy");
		return PTR_ERR(bq->fg_psy);
	}
	return 0;
}


static void fg_psy_unregister(struct bq_fg_chip *bq)
{

	power_supply_unregister(bq->fg_psy);
}

static const u8 fg_dump_regs[] = {
	0x08, 0x09, 0x0A, 0x0D,
	0x0F, 0x10, 0x16, 0x3C,
	0x3D, 0x3E, 0x3F, 0x54,
	0x55, 0x56, 0x57, 0x71,
	0x72, 0x74, 0x75, 0x76,
	0x77, 0x78,
};

static ssize_t fg_attr_show_Ra_table(struct device *dev,
				struct device_attribute *attr, char *buf)
{
	struct i2c_client *client = to_i2c_client(dev);
	struct bq_fg_chip *bq = i2c_get_clientdata(client);
	u8 t_buf[40];
	u8 temp_buf[40];
	int ret;
	int i, idx, len;

	ret = fg_mac_read_block(bq, 0x4102, t_buf, 32);
	if (ret < 0)
		return 0;

	idx = 0;
	len = sprintf(temp_buf, "RaTable:\n");
	memcpy(&buf[idx], temp_buf, len);
	idx += len;
	for (i = 0; i < 15; i++) {
		len = sprintf(temp_buf, "%d ", t_buf[i*2] << 8 | t_buf[i*2 + 1]);
		memcpy(&buf[idx], temp_buf, len);
		idx += len;
	}

	return idx;
}

static ssize_t fg_attr_show_Qmax(struct device *dev,
				struct device_attribute *attr, char *buf)
{
	struct i2c_client *client = to_i2c_client(dev);
	struct bq_fg_chip *bq = i2c_get_clientdata(client);
	int ret;
	u8 t_buf[32];
	u8 temp_buf[32];
	int i, idx, len;

	memset(t_buf, 0, 64);
	/* GaugingStatus3 register contains Qmax value */
	ret = fg_mac_read_block(bq, 0x0075, t_buf, 24);
	if (ret < 0)
		return 0;
	idx = 0;
	for (i = 0; i < 4; i++) {
		len = sprintf(temp_buf, "Qmax Cell %d = %d\n", i, (t_buf[i*2] << 8) | t_buf[i*2+1]);
		memcpy(&buf[idx], temp_buf, len);
		idx += len;
	}

	return idx;
}

static DEVICE_ATTR(RaTable, S_IRUGO, fg_attr_show_Ra_table, NULL);
static DEVICE_ATTR(Qmax, S_IRUGO, fg_attr_show_Qmax, NULL);

static struct attribute *fg_attributes[] = {
	&dev_attr_RaTable.attr,
	&dev_attr_Qmax.attr,
	NULL,
};

static const struct attribute_group fg_attr_group = {
	.attrs = fg_attributes,
};


static void fg_dump_registers(struct bq_fg_chip *bq)
{
	int i;
	int ret;
	u16 val;

	for (i = 0; i < ARRAY_SIZE(fg_dump_regs); i++) {
		msleep(5);
		ret = fg_read_word(bq, fg_dump_regs[i], &val);
		if (!ret)
			bq_log("Reg[%02X] = 0x%04X\n", fg_dump_regs[i], val);
	}
}

static irqreturn_t fg_btp_irq_thread(int irq, void *dev_id)
{
	/*struct bq_fg_chip *bq = dev_id;*/

	/* user can update btp trigger point here*/


	return IRQ_HANDLED;
}

static void fg_update_status(struct bq_fg_chip *bq)
{

	mutex_lock(&bq->data_lock);

	bq->batt_soc = fg_read_rsoc(bq);
	bq->batt_volt = fg_read_volt(bq);
	fg_read_current(bq, &bq->batt_curr);
	bq->batt_temp = fg_read_temperature(bq);
	bq->batt_rm = fg_read_rm(bq);

	mutex_unlock(&bq->data_lock);
	bq_log("RSOC:%d, Volt:%d, Current:%d, Temperature:%d\n",
		bq->batt_soc, bq->batt_volt, bq->batt_curr, bq->batt_temp);
}

static void fg_monitor_workfunc(struct work_struct *work)
{
	struct bq_fg_chip *bq = container_of(work, struct bq_fg_chip, monitor_work.work);

	fg_update_status(bq);

	fg_dump_registers(bq);

	schedule_delayed_work(&bq->monitor_work, 5 * HZ);
}


static void determine_initial_status(struct bq_fg_chip *bq)
{
	fg_update_status(bq);

	fg_btp_irq_thread(bq->client->irq, bq);
}

static int bq_fg_probe(struct i2c_client *client,
				const struct i2c_device_id *id)
{

	int ret;
	struct bq_fg_chip *bq;
	u8 *regs;

	bq = devm_kzalloc(&client->dev, sizeof(*bq), GFP_KERNEL);

	if (!bq)
		return -ENOMEM;

	bq->dev = &client->dev;
	bq->client = client;
	bq->chip = id->driver_data;

	bq->batt_soc	= -ENODATA;
	bq->batt_fcc	= -ENODATA;
	bq->batt_rm	= -ENODATA;
	bq->batt_dc	= -ENODATA;
	bq->batt_volt	= -ENODATA;
	bq->batt_temp	= -ENODATA;
	bq->batt_curr	= -ENODATA;
	bq->batt_cyclecnt = -ENODATA;

	bq->fake_soc	= -EINVAL;
	bq->fake_temp	= -EINVAL;

	if (bq->chip == BQ40Z50) {
		regs = bq40z50_regs;
	} else {
		bq_err("unexpected fuel gauge: %d\n", bq->chip);
		regs = bq40z50_regs;
	}

	memcpy(bq->regs, regs, NUM_REGS);

	i2c_set_clientdata(client, bq);

	mutex_init(&bq->i2c_rw_lock);
	mutex_init(&bq->data_lock);
	mutex_init(&bq->irq_complete);

	bq->resume_completed = true;
	bq->irq_waiting = false;

	if (client->irq) {
		ret = devm_request_threaded_irq(&client->dev, client->irq, NULL,
			fg_btp_irq_thread,
			IRQF_TRIGGER_FALLING | IRQF_ONESHOT,
			"bq fuel gauge irq", bq);
		if (ret < 0) {
			bq_err("request irq for irq=%d failed, ret = %d\n", client->irq, ret);
			goto err_1;
		}
		enable_irq_wake(client->irq);
	}

	device_init_wakeup(bq->dev, 1);

	fg_read_fw_version(bq);

	fg_psy_register(bq);

	ret = sysfs_create_group(&bq->dev->kobj, &fg_attr_group);
	if (ret)
		bq_err("Failed to register sysfs, err:%d\n", ret);

	determine_initial_status(bq);

	INIT_DELAYED_WORK(&bq->monitor_work, fg_monitor_workfunc);

	bq_log("bq fuel gauge probe successfully, %s\n",
			device2str[bq->chip]);

	return 0;

err_1:
	fg_psy_unregister(bq);
	return ret;
}


static inline bool is_device_suspended(struct bq_fg_chip *bq)
{
	return !bq->resume_completed;
}


static int bq_fg_suspend(struct device *dev)
{
	struct i2c_client *client = to_i2c_client(dev);
	struct bq_fg_chip *bq = i2c_get_clientdata(client);

	mutex_lock(&bq->irq_complete);
	bq->resume_completed = false;
	mutex_unlock(&bq->irq_complete);

	return 0;
}

static int bq_fg_suspend_noirq(struct device *dev)
{
	struct i2c_client *client = to_i2c_client(dev);
	struct bq_fg_chip *bq = i2c_get_clientdata(client);

	if (bq->irq_waiting) {
		pr_err_ratelimited("Aborting suspend, an interrupt was detected while suspending\n");
		return -EBUSY;
	}
	return 0;

}


static int bq_fg_resume(struct device *dev)
{
	struct i2c_client *client = to_i2c_client(dev);
	struct bq_fg_chip *bq = i2c_get_clientdata(client);

	mutex_lock(&bq->irq_complete);
	bq->resume_completed = true;
	if (bq->irq_waiting) {
		bq->irq_disabled = false;
		enable_irq(client->irq);
		mutex_unlock(&bq->irq_complete);
		fg_btp_irq_thread(client->irq, bq);
	} else {
		mutex_unlock(&bq->irq_complete);
	}

	power_supply_changed(bq->fg_psy);

	return 0;


}

static int bq_fg_remove(struct i2c_client *client)
{
	struct bq_fg_chip *bq = i2c_get_clientdata(client);

	cancel_delayed_work_sync(&bq->monitor_work);

	fg_psy_unregister(bq);

	mutex_destroy(&bq->data_lock);
	mutex_destroy(&bq->i2c_rw_lock);
	mutex_destroy(&bq->irq_complete);

	sysfs_remove_group(&bq->dev->kobj, &fg_attr_group);

	return 0;

}

static void bq_fg_shutdown(struct i2c_client *client)
{
	pr_info("bq fuel gauge driver shutdown!\n");
}

static struct of_device_id bq_fg_match_table[] = {
	{.compatible = "ti,bq40z50",},
	{},
};
MODULE_DEVICE_TABLE(of, bq_fg_match_table);

static const struct i2c_device_id bq_fg_id[] = {
	{ "bq40z50", BQ40Z50 },
	{},
};
MODULE_DEVICE_TABLE(i2c, bq_fg_id);

static const struct dev_pm_ops bq_fg_pm_ops = {
	.resume		= bq_fg_resume,
	.suspend_noirq = bq_fg_suspend_noirq,
	.suspend	= bq_fg_suspend,
};

static struct i2c_driver bq_fg_driver = {
	.driver	= {
		.name   = "bq_fg",
		.owner  = THIS_MODULE,
		.of_match_table = bq_fg_match_table,
		.pm     = &bq_fg_pm_ops,
	},
	.id_table       = bq_fg_id,

	.probe          = bq_fg_probe,
	.remove		= bq_fg_remove,
	.shutdown	= bq_fg_shutdown,

};

module_i2c_driver(bq_fg_driver);

MODULE_DESCRIPTION("TI BQ40Z50 Driver");
MODULE_LICENSE("GPL v2");
MODULE_AUTHOR("Texas Instruments");

Would you pls help check above debug summary and code, then support on this case? Thanks.

Best regards,

Sulyn