This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP5018: LP5018 maximum sink current

Part Number: LP5018
Other Parts Discussed in Thread: TLC59116

Dear Team,

My customer is using LP5018 for their design.

What is the difference between Maximum sink current and sink current limit?

They want to use OUT0-2 to control 9 LED.

They use 5V and 1 LED will consume around 10mA.

So the worst case will be 9 LED's(9*10mA) RGB current go to the maximum at the same time.

Which spec. should I follow?

If LP5018 is not suitable for this design, which components should I suggest to the customer?

Is TLC59116 or anything else?

Best Regards

Kevin