Other Parts Discussed in Thread: CSD95378BQ5M
Hi Team,
My customer is looking at implementing the TPS40428 for a 60A 1V design.
They have tested out the TPS40428 EVM with the CSD95378BQ5M and are seeing that the current calibration is not very accurate (going through TI Fusion GUI). For instance, they are seeing at the bottom range a current of 1.5A going through the system, when 0A is reported.
I do see an Iout cal offset in the Fusion GUI, is this recommended to use? Do we have any collateral on best practices for this?
At the top range, (over 30A) - would accuracy be in the range of +/- 3%?
Thank you!
Regards,
~John