Other Parts Discussed in Thread: BQSTUDIO
Dear All:
I use the BQ34Z100-G1 to measure the pack capacity, i have program the .Srec files into the BQ34Z100-G1, but the SOC indicator is instability , it can indicator 70% drop to 20% in the loading condition.
if you shut down the system, after 10 minutes the SOC indicator is normal with 70% What can cause the issue ?