Other Parts Discussed in Thread: LMZM23601
Hi,
The LMZM23601 EVM went damage as i check the function. After a repeated switch on the power (vin), the modul is without function.
The paramters were: Input 36V, Output 5V 1A, Last 5 Ohm || 470uF
Now the supply curent is 1,4mA and the output voltage is zero. No Bursts are to measurement at the inductor. Without a supply, i measure 1,25 Ohm between one conductor of the inductor and ground.
I think, the pull down mosfet is shorted and defekt.
Is the capacitor of 470uF to big?
Best Regards, Ben