Other Parts Discussed in Thread: BQ27500, BQ27510
Hello,
I am using the BQ27510-G3 EVM along with BQ Studio 1.3.54.1 to generate a golden image for my custom battery. Loaded default bq27510-G3_4_00.srec file into part before starting (this is my third round of trying to learn cycle). Data flash parameters all set accordingly and gauge is full access [FAS and SS clear]
I discharged the cell completely and its relaxed. According to SLUA903:
– Discharge the cell to empty and let them relax for at least 5 hours.
– Enable Impedance Track (0x21), issue a reset command (0x41). Update Status changes from 00 to 04
– Charge the cell to full ensuring that the [FC] bit gets set and let it relax for at least two hours. Qmax
updates at this point and Update Status goes to 05.
– Discharge the cell to empty using the typical discharge rate of your application. It must be between
C/5 to C/10 rate, otherwise, the learning cycle fails. Resistance tables are updated during this
discharge cycle.
– Let the cell relax for 5 hours during which the Update Status would change to 06.
I should then issue the IT command [IT_ENABLE button along right side, sends 0x21) and then RESET [sends 0x41] and update status should change to 04. When I do this, I see no change as it remains 00. I do notice that the QEN bit gets set [01 in data flash] and RUP_DIS and VOK are clear. Once charging starts, VOK sets.
Regardless of any learn cycle parameters/issues, why doesn't update status update after IT/RESET commands issued? I have started the charge cycle now. I do remember that with the bq27500 and bqeasy, UPDATE STATUS went from 00 to 01 after the charge, and then to 02 after the discharge.
Thanks,
Mike