This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dears:
There is a demand as follows:
1. DC-DC input is 18v~380v, output is 12V or 5V
2. Iout is 1.5A or 2A above.
I found the solution from reference design.
And from the PMP20745 datasheet I can see the below information, and I can not find the solution of PMP10649.
Could you kindly help to provide it?
PMP9334 30V to 350V in, 15V at 1A out
PMP7760 30V to 800V in, 21V at 1.5A out
PMP7958 300V to 600V in, 21V at 1.5A out
PMP9303 300V to 600V in, 48V at 0.63A out
PMP10606 100V to 380V in, 15V at 0.34A out, modified for non-isolated
PMP10649 49V to 450V in, 15V at 2A out
PMP20745 18V to 400V in, 15V at 0.6A out
Luck, hello and good day. Thank you for working with Texas Instruments. Please find the attached files for the PMP10649. Please let us know if you need anything else.
Best Regards,
J. Fullilove
Texas Instruments
TI Designs