Hello,
I have a question about PG pin hysteresis, V_HYS(PG).
For V_HYS(PG), only TYP value, 1%, is defined in the datasheet like the below.
Then are MIN and MAX values of this V_HYS(PG) available?
Here is the background of this question.
The threshold from PG low to PG high is defined as V_IT(PG) + V_HYS(PG).
Then because min/max values of V_HYS(PG) are not defined, we are not sure the min/max threshold values from PG low to PG high.
I believe it never happens, but no min/max definition means it could technically happen that PG never go to open drain when V_IT(PG) + V_HYS(PG) is over 100%
or PG is always open drain when V_HYS(PG) is minus %.
So my customer is requesting to add min/max to the datasheet.
Or could you show me something data to make clear min/max value?