Hi all,
Im using TPS54428 in my device under mass production as a buck converter that converts 12 V to 5 V. However, when I made a mistake such as short circuit due mechanical touching or other reasons, my 5 V rail becomes short circuited to ground. Then, I check this with my multimeter buzzer (without power on my circuit), 5 V to Gnd is connected permanently. In order to fix my circuit, I replace TPS54428 with a new one, and it works. As a result, TPS54428 does not limit its current as mentioned in datasheet and burns (This was occured in 5 devices up to now). I need your ideas or comments about this problem because there is an ongoing mass production process and I need to solve this problem. Does TPS54428 really have over current limit?
Thanks.
Best Regards