Other Parts Discussed in Thread: LM8364
Dears:
Customer will evaluate UCC28911 and have some issue as below:
A. The precision of low voltage protection.
b. The precision of current-limiting protection.
c. The precision of constant-current source.
d. What is the function of LM8364? Can UCC28911 realize the function?
Btw, the customer's project requirement as follows:
Is there any other PN to promote except for UCC28911?
1. anti shock isolation mode
2. the output power is about 10W.
3. no optocoupler primary feedback PSR
4. Integrated MOS tube (more than 700V)
5. Integrated high voltage constant current source to start
6. it is best to support CV (constant voltage) and CC (constant current) mode.
7. low power consumption, high light load efficiency
8. under-voltage protection
9. over current protection / overload protection
10. best equipped with PFC
11. over temperature protection
12. output overvoltage protection
13. short circuit protection
14. two output cross load, good voltage regulation performance.
15. it's best to have Green mode.