This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC27524: recommended common model replace ucc27517 and ucc27524, is there a

Part Number: UCC27524
Other Parts Discussed in Thread: UCC27517

projects on the demand drive current smaller 1A, 2A, 3A, replace ucc27517 and ucc27524,

is there a recommended common model?

  • Hi Eagle,

    Thanks for your inquiry, my name is Mamadou Diallo, I help support gate drivers in high power drivers' group.

    If the application does not require high current drive, consider UCC27536 with 2.5A source current and 5A sink current capability. This device does have wider supply range (VDD = 35V max) and comes in SOT-23 pin out. 

    Are you able to share the application or project where this high current is not a necessity?

    Please let us know if you require further assistance or press the green button if this helped resolve your concern.

    Thanks.

    Regards,

    -Mamadou

  • thank you!

    My application is Sloar micro inverter,Do you have any recommendations,need 1A, 2A, 3A.
  • Hi Eagle,

    UCC27536 is a good alternative but you can also control drive current by choice of Vdd supply and also increasing your gate resistor which would reduce drive current from the driver IC. Though the driver is capable of 2.5A current, it will not necessarily drive that much current if you tune this gate resistor to your advantage.

    Please let us know if you require further assistance or press the green button if this helped address your concern.

    Thanks.

    Regards,

    -Mamadou