Hello,
Copied circuit of LMR33630A from TI application notes (L is 8.2uH) except we used one 330uF Aluminum Capacitor, one 22uF ceramic one at the output. Feedback Resistors are 100k/24.9k.
Designed 24V in/5v out. Very light load.
But I got the Output of 10.5V instead 5V, and not able to be regulated. The feedback voltage is 2.14V at pin 5, showed the ratio of the Rs are correct.
What I did wrong, please?
Thanks!
Richard