Part Number: CSD16321Q5
Other Parts Discussed in Thread: TPS40007, CSD16340Q3
Dear Specialists,
My customer is considering CSD16321Q5 instead of Si4866BD and has a question.
I would be grateful if you could advise.
---
I'd like to change to CSD16321Q5 for TPS40007.
Vin:3.3V, Vout:1.2V 3.2A
Due to the specification of the controller of 3.3 V -> 1.2 V, the worst case of Vgs becomes about 2.6 V.
At this time, I think that FET may not turn ON due to variations.
Is there data that CSD16321Q5 surely turns ON under this use condition?
For example, it is helpful to have data on the maximum value of Ron at Vgs = 2.5 V.
---
I appreciate your great help in advance.
Best regards,
Shinichi