This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24103: VBAT monitoring question

Part Number: BQ24103
Other Parts Discussed in Thread: BQ24130

Hi,

We are designing a 1cell Li-ion custom battery pack.

The issue is that in order to fulfill one certification the design must pass, the battery pack shall have a set of diodes in the charge path connector and the Voltage Bat monitoring shall be current limited using a 10K resistor.

The custom battery pack simplified architecture is shown in this figure:

We have choosen the BQ241Xx IC for the charger design, due to the Bat voltage monitoring and charge is made via different pins. So the charger connector will be tied to the BAT pin and OUT pin of the BQ241xx.

Will we have any problem due to the 10K resistor or the diode stage?

Best Regards,

Juanjo