This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/UCD3138A64: How should I do for UCD3138A64 RTC_IN_1_8(pin62) when not use this function?

Part Number: UCD3138A64

Tool/software: Code Composer Studio

Hi

I find UCD3138A64 RTC_IN_1_8(pin62) have 1.8V when I measure on this pin.

How should I do for UCD3138A64 RTC_IN_1_8(pin62) when not use this function?

Short to GND, put high to VCC, configure as special function or just let this pin floating.