Hi,
What are the power sequencing requirements for the LM8342?
Ideally to simplify the sequencing requirements for my application, I would like to provide the VDD rail first and after some time apply the AVDD rail. Is this allowed or do both rails have to be applied at the same time?
Equally, will the LM8342 initialise the DC value from the EEPROM when the 3.3V rail is applied or does it need the AVDD rail present also to do this? I'm keen to avoid any delay in the VCOM output when the AVDD rail is applied.
Many thanks