Hi Team,
In the TPS650830 data sheet, there are parts that seem to be wrong.
In the equation that determines the constant of overcurrent protection of equation (3) in P.131
Is not "x1.3" necessary?, Or "IOUTMAX" instead of "IOCL"?
Reason: I think that x1.3 is 130% of "set IOCL to 130% of IOUTMAX" listed above equation (3).
However, Eq. (3) contains the IOCL, plus x1.3 is done there.
130% of IOUTMAX can be understood as IOCL.
So, if you use IOCL in equation (3), x1.3 is unnecessary, and if you use x1.3, I think that it is not IOCL but IOUTMAX.
Best Regards,
Kenji