This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62150: Controlling TPS62150 using a DAC on SS pin.

Part Number: TPS62150
Other Parts Discussed in Thread: TPS62147,

Hi there

I have looked at the application note SLVA451A and wish to use a similar control mechanism - using a DAC output to control the target voltage.

In the event that the SS pin is driven beyond 1.25V, will the target voltage dictated by the FB pin resistors be exceeded?

Thanks again