Hi,
I am using 6 of these power switches in a test fixture. Each one of these TPS24750 is used to enable power, provide current limit in the event of a short and measure the current draw of a unit under test in the fixture (the test fixture accepts 6 units for testing). The 6 TPS24750 are located on the main test board and the output of each TPS24750 is delivering the power rail of the unit under test with about 2 feet of wire. The TPS24750 is feeding 3.3V to the unit under test and it is set to current limit at 360mA. We are seeing some strange behavior when we enable the power and test the different unit under test and we are suspecting that it is related to the power. Are there any precautions or known design changes that is required on the TPS24750 when it is delivering power to a load over a run of wire?
Thanks