Other Parts Discussed in Thread: TPS51225,
Hi Sir,
I have some questions of TPS51275 and TPS51225.
1. May I know what's the biggest difference between TPS51225 and TPS51275?
I only saw the Vin(min.) and duty cycle are different.
2. Why does it show TPS51275 can regulate 4 output and Iout(max) is 20A on the website?
On the datasheet, the TPS51275 as same as TPS51225 only can regulate 2 output number and the gate driver ability or OCP parameter are the same.
3. Which device I could use?
For 5V, Iout(max) = 16.82A
For 3.3V, Iout(max) = 14.71A