Dear Sir,
We have a LED current can't be adjusted IADJ to drop 20~30% issue. LED current SPEC adjustment range= 90mA~9mA(100%~10%),Frequency: 150kHz,the PDIM is a enable LED on/off function. If device start up to adjust IADJ 60~70% stable current status can drop to 10% LED current (9mA) , If device start up IADJ setting under 30% it can't continue drop to 10% range will be keep at 30% (current 28mA) refer waveform. Normally status current must adjust up to 60% then go down 10% it's ok. Is there a suggestion to improve?
Thank you!