Hi Team,
I would like to design 5 Cells bat charger from USB PD 20V.
Consist on the flowing parts: TPS65982, BQ24610
1: Are these parts remommended for my application.
2: For Prof of consept I need Evaloation boards for both parts
As I have seen in TI Web: TPS65982 EVM Does not have the native hardware to support the 5, 9, 15 and 20V rails. Do you have anather Evaloation board that can help?
TI BU recommend using the TPS65987D for my application as it is our latest PD3.0 controller. The TPS65987EVM supports 5V, 9V, 15V, and 20V rails natively.
My Application: Battery Charger that get its power from of the shelf Power USB power PD 20V.
I shell be only Upstream Facing Port (UFP) device Sink. No need for DRP, The external PS shell be the host.
My application deal only with the USB no need to support the data USB Data signals.
Battery is made of INR18650-25R from Samsung (datasheet attached).
S= series P=Parallel |
5S1P |
Chemistry |
Li Ion Samsung |
Cell Model |
INR18650-25R |
Voltage (nominal) |
18V |
Capacity (Nominal) |
2.5Ah |
Pack Power [Wh] |
45 |
Cycles |
200-250 |
Number of cells |
5 |
. |
Allowed Current are: 0.5A up to 1.25A.
Cut off current at end of charge is 100mA.
Pre charge can be 100mA as well.
- Please Go over our Block Diagram What do you think ?
- Do you see any problem to charge 5 Cells of that battery from USB 20V?
Thanks,
Shlomi