Dear,
We are using the attached circuit to charge the battery(2 Cell Li-ion).
Now we have some concerns regarding charging voltage measured at TP49(BATTERY_PACK+ net). For eg. consider 2 cell battery voltage is 7.4V(which is also nominal voltage) now if we connect the External adapter the voltage at TP49 suddenly jumps 7.9V if we remove adapter immediately it again come back 7.4V only.This +0.50V difference observed for all other voltages also. Because of this we are unable measure the battery capacity i.e, Once the actual battery voltage reaches 7.9V the BATTERY_PACK+ terminal will show 8.4V which is max. capacity of battery. We also worried that this may also cause some damage to battery. We didn't understand why this sudden jump occurring at the BATTERY_PACK+ net.
Please reply to us if you require more data.
Regards,