Hi
customer want to get LP2985A-50DBVR output voltage VS Temperature curve @ 12V input 50mA output
but in datasheet, there is no this curve, only other input voltage curve are shown.
could you help to test and send this curve to me?
thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
customer want to get LP2985A-50DBVR output voltage VS Temperature curve @ 12V input 50mA output
but in datasheet, there is no this curve, only other input voltage curve are shown.
could you help to test and send this curve to me?
thanks.
Hi Max,
The worst-case output accuracy for the LP2985A for your customer's application can be estimated using the electrical characteristics table. For the following data, Vin = 6 V when Vout(nom) = 5 V. At Vin = 12 V the regulator's line regulation spec will reduce the output voltage accuracy.
Accuracy = Output voltage tolerance + Line regulation * delta(Vin) = 2.5% + 0.032 %/V * (12-6) V = 2.7%
As such, the worst-case output voltage range for the LP2985A is approximately 4.865 V to 5.135 V when Vin = 12 V, Vout = 5 V, and Iout = 50 mA.
Thanks,
Gerard