Since there is a worldwide critical shortage of large-value ceramic caps. We currently use a pair of 47µF 25V ceramic output caps in our TPS63061 implementation, plus a third one at a remote location, which is switched by a MOSFET. I would like to know if conventional (not polymer) tantalum caps can be used as a substitute. We can’t use polymer due to high leakage and its effect on battery life. The ones I’m looking at have ESR on the order of 600mΩ and a surge current limit of 4.8A. Would this regulator function with 300mΩ of ESR?
Best regards,
Matt