Hi,
I am trying to compile a simple program for the LP5569 using the LP5569 EVM GUI software (version 1.0.0). See below for a screenshot.
I don't understand why the compiler claims that my "wait 0.2" command is wrong. "0.2" is clearly within range of "0 to 0.484". I have tried several times, on both Windows 10 and Windows 7. I have tried writing the commands myself, and creating the program using the drop down menus under "Input Instruction". I have tried using a comma for the decimal separator. I have tried running the lasm.exe program from the command prompt directly, but I have had no luck.
Any help is greatly appreciated.
Best,
Fredrik