This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD8220: pushpull output

Part Number: UCD8220


Hi Team,

I would like to drive two FET driver ICs in the latter stage using this IC.

Expected Specification

  Frequency: 600 kHz

  Duty; 0% → 40% (fixed when reaching 40%)

  No feedback control

  No MCU controller

Is it possible to make pushpull output like attached?

Is there a reference circuit?

Best Regards,

Kenji