Hello Team,
by the CSD17585F5 is written that the maximum Vgs should be +20V. On other MOS datasheet from other vendors I do see that they do specify max +-20Vgs for an N channel MOS.
What does really mean -20V within the spec of an N MOS?
Below Vth is off so below 0 would be off. Does the CSD17585F5 support -20V without getting broken?
Can I retrieve that info from the datasheet?
Is it a different way to specify the device or it has to do with the internal structure and diodes?
Thanks,
SunSet