Other Parts Discussed in Thread: LM74610-Q1, LM74700-Q1
I have seven 12V PV panels that are to be connected in parallel to generate the current required for my application.
Each panel has it's own integral 'bypass' diode across the panel
But, to prevent illuminated panels 'driving' current into a shaded one i also need blocking diodes 'anding' the panels into a single combined 12V output.
However due to the current available from each panel, the power dissipation in conventional series diodes is too great. (even with Schottky diodes 10W for some panels)
So an 'ideal' diode is required to reduce the Vf and the SM74611 looks like a possible solution.
Looking at the datasheet I can't see any reason why the SM74611 can't be used in a 'series' application, blocking the shaded (lower voltage) PV panel from shunting the illuminated ones.
However I have not seen any applications other than the device being used as a 'Bypass' diode.
Why is this?
Am I missing something or can the device be used in a series circuit.
Please advise
Thanks
Dave