Hi
I am planning to use PTN78060W in one of our boards. The board would be powered from either 24VDC or 5VDC. So it has 3Way Power connector (terminal block)
For 24VDC Vin case
the positive of 24Vin goes straight to Vin Pin of PTN78060W that steps it down to 5V output which subsequently goes into the input of couple of more voltage regulators with 3.3V & 2V output. So no issues here
For 5VDC Vin case:
The positive of 5V goes to the track which is connected to the output pin of PTN78060W
We would not have 24V & 5V at the same time at Input. It would be one or the other
The question is that would it be safe for PTN78060W to be operated like this i.e., 5V applied at its output with Input floating for the case when our input voltage is 5V.