I am trying to use BQ26200EVM-001 and the EV2200 for monitoring the eZ430-RF2500-SEH. I did everything that the datasheet says but when i open the monitor on my computer i don't see anything. I test all the pins with a scope and i find out that the signal from the EVM2200 is (0-5 v) i thing that is not compatible RS232. My question is, do i have to convert this signal with a max232 or something like that?
Sorry if my english is not correct!