Other Parts Discussed in Thread: LM73605, TINA-TI, TPS3710
Hi, I need an application that Vin is the great 9V and IC start work and Vin is less 5V and IC shoutdown.
The R147 change to 301K ohm, R153 change to 68.1K.
The Result:
Startup (CH2:Vin, CH3:Vout, CH4:Ven):
Vin = 6.0V; Ven(UM20_PIN4):1.1V
Shutdown (CH2:Vin, CH3:Vout, CH4:Ven):
Vin = 5.4V; Ven(UM20_PIN4):0.9V