Other Parts Discussed in Thread: TPS25200, TPS2121, , TPS2553
Hello,
What is the power rating of TPS25200's RDCHG discharge resistor ?
Our application consists in using two TPS25200 and connecting their Output in order to do a logic OR. The input voltage is 5V for both.
When the first TPS25200 is disabled and the second enabled, 5V is applied on the output by the enabled TPS25200, therefore a continuous 10mA current will flow through the discharge resistor of the disabled TPS25200.
Can this current damage the TPS25200 ?
Thank you very much.
Regards.
David.