Other Parts Discussed in Thread: TPS2546
My customer is considering using our TPS2514 device. But his application only need D+D- only USB DCP applying 1.2V, current 0.9A-1.1A, But our TPS2514 could support D+D- 1.2V, and also D+ 2.7V, D- , 2.0V, current up to 2A. He do not want to use the such high current for his Apple i-phone. so I have two questions below,
1. If our device could close the D+ 2.7V, D- , 2.0V, current up to 2A setting? Or other ways to get the requirement?
2. Any other device could he use? USB DCP controller. 0.9A-1.1A
Thanks.