This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61222: How can i configure Vout=5V and Iout=150mA max

Part Number: TPS61222

I am going to have an input of 2.7v to 4.2v, I need Vout=5V and Iout=120mA for my system load.

This TPS61222 is able to give Vout= 5V max and  Iout=200mA maximum right?

How can i configure it to be Vout=5V and Iout=150mA maximum for my system load? I need some help on this based on the datasheet. Thanks.