This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/TPS630250: Regulator is heating

Part Number: TPS630250

Tool/software: TI C/C++ Compiler

Hello,

I have a custom pcb with TPS630250 and resistor are regulated to 3.0V ( R2=178k R1=500k)

Sem-T-tulo

Sem-T-tulo1

The input voltage is 3.7V if power is battery, or 5V power is USB. The output is 3V and circuit its working well but the heat is a problem because all PCB is heating.

Someone had this problem?

BR